ASUS Vivobook 17

Make every day your day

Turn everyday tasks into something special with Vivobook 17, your essential tool for getting things done easier, anywhere. It’s completely user-friendly too, with its 180 ° lay-flat hinge and physical webcam shield. ASUS Antimicrobial Guard Plus protects frequently-touched surfaces from harmful bacteria, safeguarding your health. Make all your days more enjoyable with Vivobook 17!

Performance

Power on tap

With Vivobook 17, you’re always ready to take on any everyday task, whether it’s work, play or entertainment. Whatever you need to achieve, there’s always plenty of computing power on tap with the 12th Gen Intel ® Core ™ processor, 16 GB of fast memory, 1 TB of speedy SSD storage and comprehensive range of wireless connectivity up to WiFi 6E 7 allows you to load online content in the blink of an eye.

Battery

Charge with speed

Vivobook 17 supports fast charging which allows you to charge a low battery to 60% in as little as 49 minutes 3 , so you can be up and running quicker than ever!

Display

Clearly superior display

Vivobook 17 delivers beautifully clear visuals with its three-sided slim-bezel NanoEdge display. The wide viewing angles maintain great quality even for off-center viewing, and the TÜV Rheinland eye-care certification ensures low blue-light levels that reduce the risk of eye strain during long viewing sessions.

Audio

A new perspective on laptop audio

Designed with help from the audio experts at Dirac, a professional audio solution provider, the audio system delivers the most immersive, clear, and balanced sound experience you’ve ever heard on a PC, laptop or tablet. You’ll hear a wider and deeper soundscape than you could imagine, unleashing the full audio potential of your laptop.

Optimal click ratio: Engineered to perfection

The feel of a keyboard depends on the crucial ratio between the peak force (also known as the actuation force) and the contact force. Peak force occurs when you press down on the key and reach the maximum force that the key’s underlying rubber dome can withstand without deflecting. Contact force occurs when the bottom of the key touches the circuit board to trigger an electronic signal, which in turn generates the action appropriate to the key. To achieve the most natural feel for a keyboard, ASUS keyboard experts have scientifically determined that the optimal ergonomic click ratio for a key is between 45-60%. These forces are precisely measured and tuned using the ASUS-designed rubber domes beneath the keys.

ASUS Antimicrobial Guard Plus

Inhibit 99% of COVID-19, flu virus & bacteria*

ASUS Antimicrobial Guard Plus is applied to frequently touched areas of your laptop to help keep it hygienic. This technology uses a denser treatment* that inhibits viruses and bacteria. And it is scientifically shown — using the ISO 21702 10 and 22196 11 standards — to inhibit virus and bacteria growth by more than 99% over a 24-hour period 4 . Strains used for the tests include the SARS-CoV-2 (COVID-19), H3N2 (Influenza A) and the E. coli bacterium 12 .

ASUS Antimicrobial Guard Plus

Viruses and bacteria inhibition

Viruses and bacteria are everywhere in our daily life. Antimicrobial Guard Plus inhibits all viruses and bacteria with an envelope (the outermost layer of many types of viruses and bacteria) from the surface of the protected parts. ISO 21702 testing shows that it can inhibit the growth of SARS-CoV-2 (COVID-19), H1N1, H3N2 (Influenza A) and harmful bacteria.

ASUS Antimicrobial Guard Plus

Silver ions prevents 99% reproduction

ASUS Antimicrobial Guard Plus is a surface coating 20 on the laptop 21 that contains positively-charged silver ions. Silver ions and negatively-charged microbial cells are attracted to each other and then pierce the surface to damage their structure, inhibiting reproduction.

Connectivity

Perfect in every detail

Vivobook 17 keeps you fully connected with its comprehensive I/O ports. There are one USB-C ® 3.2 Gen 1 port, two USB 3.2 Gen 1 Type-A ports, a USB 2.0 port, HDMI ® output and an audio combo jack — so it’s easy to connect all your existing peripherals, displays and projectors.

Military-grade

World’s most strictly tested US military-grade laptop durability 22

ASUS laptops 6 are engineered with extraordinary toughness meet the exacting US MIL-STD-810H military-grade standard, undergoing 12 rigorous test methods and 26 punishing test procedures — exceeding industry standards. The upshot is a range of products that are renowned for reliability and durability. These factors also inherently benefit longevity and thus sustainability, so you can work, travel or relax with the confidence that your ASUS laptop is ready for the real world — today, and long into the future.