ORBIT 960

The Orbit 960 is a 4K ultra high definition recording with clarity and reliability. Empowered with the Sony Starvis sensor and driver assist features.

The Orbit 960 is a 4K ultra high definition dash cam to record videos at a resolution of 3840 x 2160p at 30fps, ensuring clarity and quality. The 2.7” LCD screen will give you easy visibility to access your dash cam menu and footage. Recording at a 140° wide angle lens, this allows drivers to record more lanes of the road, catching all the important details such as license plates. Revolutionary night vision technology is built-in using the Sony Starvis sensor. Rendering a more well-lit and sharp video while in low light situations. Wi-Fi capability is enabled to for instant file viewing, transferring, and sharing directly from your dash cam to smartphone. Equipped with GPS logging to help drivers track the speed and all incident locations. Additionally, driver assist features can be turned ON to give you a driver fatigue warning and headlight reminder. The built-in G-Sensor will lock onto emergency files if it senses a collision, so you won’t need to worry about files being loop recorded over. With a max capacity of 512GB drivers won’t need to worry about limited storage. A 16GB micro SD card is included within the package, so you’ll be set to capture everything that unfolds on the road.

4K ULTRA HIGH DEFINITION VIDEO

The Orbit 960 can record videos at a resolution of 3840 x 2160p at 30 fps. Empowered with ultra definition, record in clarity and quality while driving at high speeds. No longer will you need to worry about missing those small important details such as license plates.

NIGHT VISION WITH SONY STARVIS SENSOR

A 120° viewing angle will allow the dash cam to capture more lanes on the road. This will help users capture those small details, such as license plates.

WI-FI FOR INSTANT FILE SHARING

For a more user-friendly experience, Wi-Fi capability is now enabled on the dash cam. Users can instantly view, transfer, and share their footage from their dash cam straight to their smartphone within minutes once connected to the GEKO App. Easily share your footage with your friends, family, and the police.

GET READY TO BE AMAZED

GPS LOGGING

GPS logging will record the accurate speed and location information from the dash cam and when the car is in motion. This can be vital information in pinpointing the exact location where an incident happened which can be crucial in an insurance claim.

DRIVER FATIGUE WARNING

Drivers can set a time for a alert reminder to take a break from driving if they have been driving for a long period of time.

BUILT-IN G-SENSOR

G-sensor is built into the dash cam, so if it senses drastic breaking or a collision, it will automatically lock onto the emergency files. This ensures that these files will not be loop recorded once they have been locked.

2 MOUNTING OPTIONS

The Orbit 960 has 2 mounting options, suction cup and a 3M stick tape mount. Users will have the option of choosing the mount that works best for their vehicle.

SUPPORTS 512GB WITH 16GB
MICROSDINCLUDED

The Orbit 960 supports up to 512GB of external storage, so there is no need to worry about limited space for footage. Additionally, a 16GB microSD card is included in the package, so you’ll be set to install the Orbit 960 in your car and start recording.

LIFETIME OF FIRMWARE
UPDATES

Keep your dash cam up to date with the latest firmware and updates. All you need to do is check our website regularly for new available updates found in the support tab.