The datAshur PRO USB 3.2 Gen 1, PIN authenticated, hardware encrypted flash drive is the perfect solution for storing your personal or company data.

OS and platform independent

No software required. Works on any device with a USB port!

Compatible with: macOS, iPadOS, Windows, Linux, Chrome OS, Android, Thin Clients, Zero Clients, Embedded System, Citrix and VMware

FIPS PUB 197 validated encryption algorithm

Employing AES-XTS 256-bit full disk hardware encryption, the datAshur PRO seamlessly encrypts all data on the drive whilst at rest, keeping your data safe even if the flash drive falls into the wrong hands.

Independent user & admin PIN

Which makes it perfect for corporate and government deployment. If the user forgets their PIN, the drive can be unlocked by the admin PIN, the admin can then allow the user to set a new PIN.

Autolock

The datAshur PRO automatically locks when unplugged from the host computer or power to the USB port is turned off and can also be set to automatically lock after a predetermined amount of time.

The datAshur PRO is intelligently programmed to protect against all forms of brute force attacks. If the user PIN is entered incorrectly 10 consecutive times then the user PIN will be deleted. All your data will remain on the device but now you can only access it by entering the admin PIN.

However, if you enter the admin PIN incorrectly 10 consecutive times, the PIN, encryption key and data will be lost forever. The device will revert to the factory default settings and will need to be formatted before use.



Safeguard your valuable and sensitive data

The datAshur PRO securely encrypts, stores and protects data to ensure compliance with stringent regulations such as GDPR, HIPAA & CCPA.