Encourage interactive classrooms and engaged learning with StarTech.com mobile sit-stand workstations.
These sit-stand desks allow students to set up their learning environments to suit their needs. The workstations can easily be adjusted from a sitting position to a standing position with no disruptions to the class. Teachers can arrange and rearrange their classrooms according to their lessons, they can set up individual desks for tests or lectures, or group two or more desks together for projects. The two front casters can be locked in place to prevent the workstations from moving.
Simple height adjustments for individualized comfort
Moving between sitting and standing throughout the day brings many health benefits, from increased circulation to reduced fatigue. The sit-stand workstations make it easy for students to change their positioning throughout the day, keeping them attentive and focused. Giving students the freedom to stand when needed can also help to reduce anxiety and restlessness.
Students can adjust the desk to any height between 31.75" (806.45 mm) and 45" (1150 mm), they simply need to squeeze the lever located under the work surface, and then move the workstation up or down. The adjustment lever on the right side of the desktop can also be locked using the provided key, so that the height won't accidentally change if a student knocks the lever.
There are no preset heights, so each student can find the precise height they need to work most comfortably.
Large work surface sized to fit student needs
The large surface area of the desktop, 24" (600 mm) x 31.5" (800 mm), provides ample room for all schoolwork and supplies such as textbooks, pens, and other stationery.
For laptop configurations, the workstations feature cable clips that run down the column in order to help keep cables organized. The workstations can also be combined with monitor mounts" append_qs="filter_NUMOFDISPLAY=1 to add displays. The work surface also provides enough room for a keyboard and mouse.
Note: If more than 10 lb. (4.5 kg) of weight is added to the work surface, some manual force will be needed to raise the desktop.
Mobile desks, perfect for customizable classrooms
Teachers can create dynamic environments to accommodate different needs. They simply need to unlock the two front casters and move the workstations around the classroom to:
Teachers can also use the workstations for presentation purposes. The mobile workstations are ideal for moving around from class to class with laptops and other tools, and the height can be adjusted and locked.
The portable desks can also be used in the following settings:
The STSCART is backed by a StarTech.com 2-year warranty and free lifetime technical support.