The LinkRunner AT Network AutoTester is available in two models: LRAT-2000 and LRAT-1000.
LinkRunner AT 2000 features include*:
*These exclusive features cannot be added to the LinkRunner AT 1000.
The LinkRunner AT offers user-configured auto-tests for a wide range of important tasks. This network tester’s quick cable test and switch identification facilitates fast problem isolation. Test results can be automatically uploaded to the Link-Live cloud service to improve collaboration between network engineers and technicians, creating greater job visibility, project control, and fleet management. Validate vital functions of copper or fiber Gigabit Ethernet links in less than 10 seconds with the comprehensive AutoTest.
“I was amazed... this device was finished testing before I could even explain to one of my junior engineers what I was actually doing. I’ve been an engineer for more than 20 years and this device just gets me, it understands what my workflow truly is and what type of information I need to do my job.” Charles Morris, senior consultant at ACS, A Xerox Company
“After using the LinkRunner AT I can unquestionably say it will save this organization time and money while improving satisfaction. In fact, now that I’ve used it, I wouldn’t want to be without one.” – Thomas Franchina, Senior Systems Programmer, United Health Services
“Not only is the LinkRunner AT fast, but it’s incredibly thorough with the essential Ethernet connectivity tests I need. So while it speeds troubleshooting, it also gives me a high level of confidence in the results. If the unit says the connection is okay, I know it’s okay.” – John Heidelberg, Network Administrator, Jensen International
"This new tester speeds up troubleshooting as I never would have imagined.... especially for the price! For example you go to a station, plug it in, and in a few seconds you know not only that you have a link up, but you know the switch name that it's connected to, the switch port, the VLAN, etc. This is a huge time saver! Simply tracing a cable that is not labeled... or worse that is labeled wrong, can take hours. But with the LinkRunner AT1000 you know all the details... in a few seconds! I simply love it! Don't leave home without it!" – Guillaume P., Technician, BroadNetworx
AutoTest runs a set of connectivity tests in seconds
With a three second startup and a user-defined AutoTest that performs your required set of connectivity tests in seconds, the LinkRunner AT network tester enables you to quickly and accurately identify and solve network problems.
1 Gig link on copper with PoE on port 30, 1 Gig link on fiber on port 6
The LinkRunner AT displays critical nearest switch information including:
PoE Setup
You can quickly validate PoE performance by drawing actual power up to the 802.3at standard 25.5W. Load the circuit to stress switches, cabling and patch panels, all while measuring the voltage and pairs being used. The ability to validate the TruePower delivery before installing cameras, APs and phones ensures smooth deployment.
IP Addresses
Validate the IPv4 DHCP auto-negotiation process, subnet and DHCP server. Verify IPv6 Link-Local and Global addressing.
Ping & TCP Port Connectivity
The LinkRunner AT performs either a Ping or a TCP port open test to verify connectivity. The connection to the default Gateway, preferred DNS server and alternate DNS server is tested, including response time. The connection to up to 10 user-defined target devices, servers or services is tested using Ping or a user-defined TCP port number. Results include response time and IP address if a URL was used as a target.
MAC ACLs can be validated using MAC spoofing.
Verify access to secure networks using 802.1x and MAC Access Control Lists (ACL). The included LinkRunner AT Manager Software can be used to configure 802.1x EAP type, download certificates, and enter passwords.
LinkRunner AT 2000 supports packet reflection for:
Cable Location
Locate cable runs with toning, switch port advertisement, switch port link light blinking, and remote cable identifiers. Toning supports both analog and digital IntelliTone modes.
Easily find opens, shorts, miswires, and split pairs three different ways:
Good cable including length
A mis-wired cable with pairs 1,2 and 7,8 swapped using cable identifier #4
A cable with an open on 4 using the built in wiremap port
A mis-wired cable with pairs 3,6 & 4,5 split
The LinkRunner AT fully supports multiple languages including English, French, German, Spanish, Portuguese, Russian, Japanese, and Simplified Chinese. Multi-language support included the LinkRunner AT user interface, getting started guide, user manual and supporting LinkRunner AT Manager software, help files and user reports.
LinkRunner Family Comparison Chart
LinkRunner AT is available in two models: LRAT-2000 and LRAT-1000. LinkRunner AT 2000 adds the following exclusive* features:
*These exclusive features cannot be added to the LinkRunner AT 1000.
Link-Live Cloud Service provides IT Managers and Engineers a centralized cloud-based platform for collecting, managing, and analyzing test results and site data uploaded from NetAlly network testing tools. This provides organizations with the ability to easily provide proof-of-performance and better manage jobs and staff efficiency. It speeds network documentation, sharing of data and reduces duplication of effort through improved visibility and collaboration between field technician and remote engineers. An API is available to retrieve and integrate data in Link-Live to corporate systems, such as a trouble-ticket system or network management system.