So capable, you wont want to put it down. So thin and light, you wont have to
With iPad, weve always had a somewhat paradoxical goal: to create a device thats immensely powerful, yet so thin and light you almost forget its there. A device that helps you do amazing things, without ever getting in your way. iPad Air 2 is all that. And then some.
Not just a thinner display. A beautiful display
To create the astonishingly thin silhouette of iPad Air 2, we started by redesigning the Retina display, fusing what had been three layers into one. Not only did this make the display thinner, it made it better, with more vivid colors and greater contrast. Then we added an antireflective coating, giving iPad Air 2 one of the least reflective displays of any tablet in the world.
Massive power. In a minimal form
Not only is iPad Air 2 thinner, its also a lot more powerful. We designed a chip, the A8X, that delivers substantially better CPU and graphics performance than its predecessor. In fact, with its 64-bit desktop-class architecture, iPad Air 2 is as powerful as many personal computers. Its power efficient, too, with a 10-hour battery life that lets you work, play, surf, and shop all day long.
Advanced security. Right at your fingertip
iPad Air 2 comes with our breakthrough Touch ID technology. It gives you an unprecedented level of security because it uses natures most perfect password: your fingerprint. So with just one touch, you can instantly unlock your iPad Air 2. But Touch ID goes beyond that. You can also make secure purchases in iTunes, iBooks, and the App Store. And with Apple Pay, you can unlock an entire world of online shopping thats fast, convenient, and secure.
Two amazing cameras. Cleverly disguised as an iPad
The iSight camera in iPad Air 2 delivers advanced optics, an improved sensor, and a powerful Apple-designed image signal processor. There are features like panorama, time-lapse videos, slo-mo, and burst and timer modes. The front-facing FaceTime HD camera has been redesigned, too, with an improved sensor and larger pixels for even better low-light performance. The upshot? All your photos and videos and video calls and selfies look incredible.
Faster wireless. Good things come to those who dont wait
Wi-Fi on iPad Air 2 is fast more than twice as fast as the previous generation so downloading movies and streaming videos take less time. And the Wi-Fi + Cellular model is equipped with faster, more advanced LTE technology. In addition, the cellular model lets you choose from a variety of carriers and flexible short-term plans. So you can make fast connections, even when youre on the go.
Apps designed for iPad.
And everything you want to do with it
iPad Air 2 comes with powerful apps for the things you do every day, like surfing the web, checking email, editing movies and photos, writing reports, and reading books. And there are hundreds of thousands of apps on the App Store, designed specifically for the large Retina display (instead of stretched-out phone apps). So whether its photography, gaming, traveling, or managing your finances, youll find an app that will help you do it better.
A better experience with every touch
iPad Air 2 runs iOS 9, the most intuitive, advanced and secure mobile operating system in the world. If it feels like iOS 9 was made for iPad, its because it was. With improved apps and new features like Slide Over, Split View, and Picture in Picture, iOS 9 helps you get more done in powerful yet simple ways. Whether youre checking messages while answering email or creating a presentation while watching the big game, iOS 9 helps you get more out of iPad than ever before.