High Performance USB 3.0 Drives

For transferring data between devices, you really can’t beat a USB drive. With the introduction of USB 3.0, transfer speeds have significantly increased and with drives can hold as much as an entire computer due to higher storage capacities. And naturally, some USB 3.0 drives are faster than others. High performance USB 3.0 drives are distinguished from standard USB drives by higher read/write speeds. Since they are faster they work especially well for large files, such as raw photos, video files, or a large data library. Photographers, videographers, and data analysts especially will appreciate the fast data transfer speeds and high storage capacity. With a high capacity USB 3.0 drive, you can virtually hold all your computer’s data files in the palm of your hand.
High Performance USB 3.0 Drives

<b>The USB 3.0 Interface</b></br> The USB 2.0 interface was limited in that it supported data rates up to 480Mb/sec, whereas the USB 3.0 interface supports up to 5Gb/sec, approximately 10 times the speed potential of the older USB 2.0 interface. Newer USB 3.0 flash drives allow users to take advantage of the higher performance potential of the USB 3.0 interface. In addition to being faster, the USB 3.0 interface provides more power for device charging and is backwards compatible with USB 2.0 devices.
The USB 3.0 Interface
The USB 2.0 interface was limited in that it supported data rates up to 480Mb/sec, whereas the USB 3.0 interface supports up to 5Gb/sec, approximately 10 times the speed potential of the older USB 2.0 interface. Newer USB 3.0 flash drives allow users to take advantage of the higher performance potential of the USB 3.0 interface. In addition to being faster, the USB 3.0 interface provides more power for device charging and is backwards compatible with USB 2.0 devices.
<b>Speed</b></br> Is a high performance USB 3.0 drive actually faster than a standard USB 2.0 drive?  The short answer – absolutely!  Verbatim’s high performance USB 3.0 drives use dual-channel architecture to increase data transfer speeds.  Compared to single-channel drives, dual-channel USB 3.0 drives can transfer data up to twice as fast.  Single channel drives can only read or write data onto one flash memory IC (Integrated Circuit) at a time.  Dual channel drives can read or write data onto two flash memory IC’s at the same time, effectively doubling the data rate.
Speed
Is a high performance USB 3.0 drive actually faster than a standard USB 2.0 drive? The short answer – absolutely! Verbatim’s high performance USB 3.0 drives use dual-channel architecture to increase data transfer speeds. Compared to single-channel drives, dual-channel USB 3.0 drives can transfer data up to twice as fast. Single channel drives can only read or write data onto one flash memory IC (Integrated Circuit) at a time. Dual channel drives can read or write data onto two flash memory IC’s at the same time, effectively doubling the data rate.
<b>Compatibility</b></br> If you recently bought a new computer, chances are your computer is equipped with one or more USB 3.0 ports.  Using a USB 3.0 drive with a USB 3.0 port allows you to take advantage of additional performance the USB 3.0 interface has to offer, while still being compatible with USB 2.0 drives.  You can also use your USB 3.0 drives in older USB 2.0 ports, although the performance will be lower. For maximum speed and performance, use your USB 3.0 drive with a USB 3.0 port.
Compatibility
If you recently bought a new computer, chances are your computer is equipped with one or more USB 3.0 ports. Using a USB 3.0 drive with a USB 3.0 port allows you to take advantage of additional performance the USB 3.0 interface has to offer, while still being compatible with USB 2.0 drives. You can also use your USB 3.0 drives in older USB 2.0 ports, although the performance will be lower. For maximum speed and performance, use your USB 3.0 drive with a USB 3.0 port.

Store 'n' Go V3 Max USB 3.0 Flash Drive
Store 'n' Go Vx400 USB 3.0 Flash Drive
High Speed USB 3.0 Controller
Dual Channel Interface
Flash Type
TLC
MLC
Available Colors
Blue
Silver
16GB
32GB
64GB
128GB
256GB
Transfer Speed MB/sec
Up to 175MB/sec
Up to 400MB/sec