Active Stylus for Smartphones and Tablets

With today's ever-shifting transformation towards a paperless world, we rely more than ever on our electronic devices to carry out daily activities such as sending emails, taking notes or running businesses. IOGEAR's PenScript™ Active Stylus sets out to redefine the way we interact with our touchscreen and mobile devices.

Break free from the standard, large rubber tip stylusses, with the PenScript's precise 1.9mm POM tip:

  • Unparalleled accuracy
  • Glides effortlessly over glass displays
  • Actively responds to touch-detection

The sleek design with integrated rubberized grip fits naturally into the hand for comfort while you draw, write, and navigate through your tablet or smartphone.

What is an Active Stylus?

An active stylus is an input device that allows the user to write or draw directly on a device's screen. It is usually used for precise drawing, note-taking, annotating electronic documents or providing electronic signatures. Active styluses have evolved from older inactive styluses that contain no electronic components and feature a large rubber conductive tip that lacks the accuracy and features that an active stylus, such as the IOGEAR PenScript™ provides.

The Next Generation Stylus

The PenScript™ works by generating electric signals that are picked up by your device's built-in digitizer. These signals are then transmitted to the device's controller which in turn senses the pen's location, pressure, and other functionalities. IOGEAR's PenScript utilizes Power Tip Technology™ to pinpoint the exact location of the stylus tip on the touchscreen providing both fluidity and exceptional accuracy when writing or drawing.

Thoughtful Design, Unparalleled Performance

The IOGEAR PenScript™ was designed with one thing in mind - how do we design a stylus that simulates the seamless pen-on-paper writing experience? Through research and development, IOGEAR decided to use premium quality materials and a very small and precise 1.9mm stylus tip made of POM (polyoxometalate). The POM material minimizes friction and allows the stylus to glide effortlessly over glass displays much like how a pen glides over paper.

The body of the stylus is made of a high-grade anodized aluminum alloy that not only gives the stylus a beautiful look and feel, but also provides durability and rigidity. In addition, the integrated rubber grip is thoughtful and adds to the pen-like feel of the PenScript™. The result of all these features is a well-balanced writing utility that not only feels great in the hands, but defines a new level of performance, control and reliability among styluses.

Stylus Gaming

The PenScript's fine point tip gives mobile gamers the advantage because it provides more precision, a higher level of accuracy and a larger field of vision compared to the fingertip.

Use the fine tipped stylus for precision drawings, photo editing, aiming while shooting targets or quick, effortless navigation through games.