Wireless Gaming Keyboard & Mouse

Kaliber Gaming's new GKM602R Wireless Gaming Keyboard and Mouse Combo offers both gamers and desktop users a great way to "cut the cord," while also providing key features for when it's time to get your game on. The 2.4GHz wireless connection allows working from a distance, so you can play games from the sofa or work in a conference room without being tethered to the computer.

Ultra-Durable Keyboard With Innovative Diamond Ring Keycap

The GKM602R's innovative Diamond Ring Keycap structure provides a solid stroke, free of the lateral play or "slop" common to other keyboards. The 8 anti-ghosting keys ensure the most important keystrokes are always accurately read, even when you're mashing multiple keys at the same time. Even when mashing keys, the durability of the GKM602R keyboard switches are rated for over 20-million cycles, so you can count on years of hard-use service.

The 7-Button Precision Gaming Mouse

The included 7-button precision gaming mouse features three programmable macro buttons and an adjust on-the-fly DPI button that is perfect for shifting between speedy movement and controlled aiming. To stand up to the rigors of online gaming, the GKM602R mouse features Omron 10-million cycle switches inside the mouse.

Mouse Configuration Software

The GKM602R's free downloadable configuration software allows programming custom functions for three of the mouse's seven buttons. With a single press of a macro button you can execute commands that would normally be much more difficult, and gain a huge advantage over the competition. Change semi-automatic weapons to fully automatic by setting a macro with incredibly short time gaps between button presses. Set mouse buttons to use the melee weapon, throw grenades, crouch, change weapons, etc. - all without using the keyboard so you can keep your fingers glued to the WASD keys.

Water-Resistant Keyboard

The GKM602R Gaming Keyboard features a water-resistant design with bottom openings that allow spilled liquids to drain harmlessly through the keyboard. Now don't go pouring your two-liter bottle of soda into the keyboard just yet- sure, the keyboard can take it, but the sticky mess left over isn't exactly helpful in winning those big online battles.

Great For Non-Gamers Too

Although intended for casual gamers and users that split time between work and play, non-gamers will benefit from a boost in productivity when using the Kaliber Gaming GKM602R Wireless Gaming Keyboard and Mouse Combo. Aside from gaming functions, the GKM602R mouse's configuration software turns the three macro buttons into powerful tools. Each can act as hotkeys or command keys, control media playback, activate keyboard macros, insert text strings or function as direct links to make your most common desktop tasks more efficient. Each of the mouse's macro buttons can be independently programmed to act as any of the above options. With the ability to quickly switch between up to eight profiles you can have a total of 24 custom functions ready to use for anything from document writing, photo editing, coding, drawing, and more.

The GKM602R mouse's programmable macro buttons offer customizable convenience that anyone can use. Photoshop users can set up buttons to quickly open palettes, run filters, activate batch processes, etc. Web surfers can use the macro buttons for commands like back, forward and next tab for added convenience. AutoCAD and Solidworks users can set their favorite tools and functions to a macro button, speeding up the design process. No matter what you do the GKM602R software can make it easier, faster and more convenient.

Pair It With Keymander To Destroy The Competition

Are you a console gamer? Did you know that instead of the joystick controllers you can use a keyboard and mouse with most games by connecting through a mouse & keyboard adapter like IOGEAR’s Keymander? Using the GKM602R Wireless Gaming Keyboard and Mouse Combo with Keymander offers a gaming experience on your PS4, PS3, Xbox One or Xbox 360 that simply cannot be matched with a standard controller. Precision aiming, faster targeting and easier movement while shooting are just a few of the reasons computer gamers have always had an advantage over console gamers.