Anytime, Anywhere, Wireless Network Monitoring and Wi-Fi Troubleshooting with the AirMagnet WiFi Analyzer Pro
The AirMagnet WiFi Analyzer PRO automatically detects and diagnoses dozens of common Wi-Fi network performance problems, security threats, and wireless network vulnerabilities, enabling IT staff to quickly solve end-user issues. This tool detects throughput issues, Wi-Fi connectivity problems, device conflicts, signal multipath issues and much more – and features a full compliance reporting engine, including wireless PCI, SOX, and ISO.
WiFi Analyzer is the industry standard Wi-Fi analysis and monitoring software tool for mobile monitoring, auditing and Wi-Fi troubleshooting enterprise WiFi networks.
Never Miss Any WiFi Traffic
With AirMagnet Wi-Fi Analyzer, you have the ability to capture any Wi-Fi traffic for 802.11a/b/g/n/ac networks, including the latest 3 X 3 802.11ac traffic. With this ability you never miss any Wi-Fi traffic, which allows you to solve any Wi-Fi network troubleshooting problems right the first time without costly rework or escalations.
Built-In Wireless Expertise
The AirWISE® engine automatically detects the root cause of dozens of wireless network troubleshooting issues across the spectrum AirWISE® eliminates the need for users to manually interpret complex packet decodes and wireless data by taking the proactive role of identifying and explaining more than hundreds of threats and performance issues before they impact the Wi-Fi network. The user-friendly AirWISE® interface explains alarms in straightforward details, provides access to additional diagnostic data, and offers advice on corrective actions.
WLAN Client Roaming Analysis
Ensuring a smooth roam between AP’s, without any dropped calls or sessions and in a way that is not noticeable to the user is key for any deployment. AirMagnet WiFi Analyzer PRO leverages support for multiple WLAN adapters plugged into the computer to troubleshoot client roaming issues – one of IT staff’s most commonly reported problems for WLAN networks.
AirMagnet WiFi Analyzer provides advanced details on all roaming transactions for any WLAN client. Users are powered with AirWISE® expertise to get detailed reasons for the roaming event taking place, device and channel parameters that influence the roam, and visibility into whether the roam was good or not.
For VoWLAN phones, users can monitor voice delays and other statistics as the phone roams from one AP to another in the middle of a conversation. The application provides VoFi-specific data (such as WiMOS, Signal Strength, etc.) leading up to the attempt, and packet transmission rates for the conversation.
Complete Wi-Fi Interference Detection & Wi-Fi Analysis
Interference is one of the leading causes of poor connectivity and performance problems in the network. This interference can be from other Wi-Fi devices, poor channel planning (adjacent or co-channel interference), or from non-Wi-Fi interference sources. Wi-Fi interference occurs as a result of co-channel/adjacent channel interference from the corporate or neighbor’s WLAN, hidden nodes in the environment, or non-Wi-Fi devices operating in the 802.11 band. AirMagnet WiFi Analyzer’s interference status indicator lists the overall interference status for each Wi-Fi channel, which is based on the Wi-Fi interference score for the devices contributing to the interference. It also provides a list of hidden nodes and non-Wi-Fi devices (non-Wi-Fi detection requires AirMagnet WiFi Analyzer PRO and AirMagnet Spectrum XT to be installed on the same machine) operating in the channel. This enables users to easily plan future Wi-Fi deployments or modify their existing deployment to minimize interference and, in turn, improve network performance.