Product Details
![]() |
Clean and disinfect in one efficient wipeSometimes clean just isn’t enough. That’s why Clorox® Disinfecting Wipes are made to kill 99.9% of viruses and bacteria, including Staph, E. coli, Salmonella, Strep, Kleb and the viruses that cause colds and flu.Clorox® Disinfecting Wipes give you all kinds of multi-tasking power in one wipe, ready to attack multiple surfaces, multiple messes and all manner of nasties you find lurking in your home.* Human Coronavirus, Influenza A2 Virus,Staphylococcus aureus, Escherichia coli 0157:H7,Salmonella enterica, Streptococcus pyogenes,Klebsiella pneumoniae | ![]() |
Multi-purpose means multi-surface
You want to keep all the surfaces in your house clean and disinfected, from appliances and countertops, to doorknobs and toys. That’s why our wipes are specially formulated to be safe on hard, nonporous surfaces such as sealed granite, sealed hardwood, stainless steel, glass, plastic, tiled walls and floors, and more.![](https://content.etilize.com/rich-marketing/en_us/1010898155/UWqJ3tTfThekaH8TUemQ_14365485105353.jpg)
Clorox® Disinfecting Wipes have a unique clear-drying formula that makes them especially effective for cleaning and disinfecting shiny surfaces like glass tables, bathroom mirrors and metal fixtures. And while they may be gentle on surfaces, Clorox® Disinfecting Wipes are tough on the grease, dirt, grime and soap scum that stand in the way of a healthy shine.
![](https://content.etilize.com/rich-marketing/en_us/1010898155/wRo3oxlQsS0Y18RlOr5l_14365485105354.jpg)
Handy in the house or on the go
Germs and grime know no boundary. That’s why Clorox® Disinfecting Wipes are ready for anything. Keep them handy for high-traffic areas like kitchens and bathrooms, and for germ magnets like doorknobs and faucets. Put them to work on window blinds, toy boxes, coffee tables, dining tables and handrails. Take them on the road to clean and disinfect steering wheels and car seats, grocery carts and airplane tray tables. Keep a canister handy in your office, gym and child’s day-care center.![](https://content.etilize.com/rich-marketing/en_us/1010898155/uQHsf9rcQoK8xbGjYoEX_14365485105355.jpg)
How to Use
Clorox® Disinfecting Wipes clean and disinfect at the same time. When you use a sponge, dishrag or even paper towel, you can spread bacteria from one surface to another. Instead of killing germs, you are pushing them around and possibly increasing the contaminated area.![How to Use](https://content.etilize.com/rich-marketing/en_us/1010898155/pYSpQxtVS2jEHzbO3pkQ_14365485105356.jpg)
To Clean: Remove excess dirt. Wipe surface clean with Clorox® Disinfecting Wipes. Let surface dry. To Disinfect and Deodorize: Remove excess dirt. Wipe surface, using enough wipes for the treated surface to remain visibly wet for 4 minutes. Let surface dry. For surfaces that may come in contact with food, like appliance interiors, a potable rinse is required. Clorox® Disinfecting Wipes should not be used for personal cleansing or as a baby wipe. Dispose of wipes in the trash after use.