AKRacing Masters Series Max Gaming Chair
Introducing Max by AKRacing – The tank of a gaming chair!
Crafted for big & tall, AKRacing Max is the tank of a gaming chair, according to PCMag. It combines AKRacing best-selling looks with XL parts. It features a wider frame, an upgraded mechanism and a custom gas lift with a maxed out weight capacity of up to 400 lbs, making it the only true big man's chair on the market. Rock It and Lock It mechanism lets you lock the chair in any desired tilt position. Just like all other AKRacing chairs, Max boasts top-quality pleather upholstery, all-metal frame, 55 kg/m3 cold-cure foam padding and adjustable headrest and lumbar support pillows for comfortable seating. All of that functionality sits atop a five-star aluminum base, steel frame, and large 2.5-inch casters.
4D Adjustable Armrests
AKRacing Masters Series Max gaming chair features 4D armrests adjustable in 4 directions: up & down, back & forth, rotating to the sides and sliding in & out.
AKRacing Masters Series Max boasts a flat wide seat, which makes this chair perfect for big & tall people, providing additional space for relaxed seating.
AKRacing Masters Series Max gaming chair features a custom heavy duty gas lift rated up to 400 lbs, unlike other big & tall chairs on the market, which use class 4 gas lift (rated only up to 330 lbs).
AKRacing Masters Series Premium gaming chair sits on a 5-star advanced high tensile strength molded aluminum base, which is about 10 times stronger than steel, and features 2.5 inch PU wheels that roll easily on all kinds of surfaces.
All AKRacing gaming chairs have a full 180 degrees recline, compared to only 120-135 degrees recline offered by other gaming chair brands.
AKRacing Masters Series Premium gaming chair features an advanced mechanism with Rock It & Lock It function, allowing to rock in the chair, adjust the rocking tension and also lock the chair seat at an angle for ultimate comfort while gaming, working or just relaxing.
AKRacing chairs are covered by a stress-free market-leading warranty. Upholstery, foam and parts are covered for 5 years, while the metal frame is covered for 10 years. Friendly US-based customer service, no hidden service and shipping charges, or restocking fees. Support available via toll-free phone, email, social media, or official AKRacing website.
AKRacing has been in business since 2001 as a real seat manufacturing company. First in automotive sport seats, then expanding to gaming and office chairs. We do 100% of our own design, R&D, product development, testing and quality control. We are sure no one makes a better gaming chair – that is why we back it with a 5 year warranty for the chair and 10 years on the frame.
Racing Heritage
AKRacing has started as a real race car manufacturer in 2001. With our heritage in the racing industry, AKRacing knows cutting corners is never welcome. We take this concept seriously when it comes to our chairs, too. Our design philosophy dictates a minimum standard for a true performance chair.
AKRacing Factory
AKRacing is one of only a few gaming chair companies that owns its own factory, meaning our chairs are created in-house, from design to manufacturing to tooling our own armrests and bases, and undergo strict quality control.
Quality & Craftsmanship
AKRacing sources premium quality materials for its products and takes pride in its dedication to artistry and craftsmanship. From premium grade PU leather and top grain leather for chair upholstery, to steel frames treated with high performance anti-corrosion topcoat, you can see the hand of the artist in every chair produced by AKRacing.
AKRacing at Fortnite Pro-Am Tournament
AKRacing is the official gaming chair sponsor of the Epic Games' Fortnite Pro-Am tournament featuring 50 celebrities and 50 gaming influencers.
AKRacing at Zotac Cup Masters: Starcraft Remastered
AKRacing is the official gaming chair sponsor of Zotac Cup Masters: Starcraft Remastered.
AKRacing at TwitchCon 2017
AKRacing is the official gaming sponsor of TwitchCon 2017
AKRacing at H1Z1 Pro League
AKRacing is the official gaming chair sponsor of H1Z1 Pro League battle royale eSports competition at Caesars Entertainment Studios in Las Vegas.
AKRacing at H1Z1 Pro League
AKRacing is the official gaming chair sponsor of H1Z1 Pro League battle royale eSports competition at Caesars Entertainment Studios in Las Vegas.
AKRacing at PUBG Global Invitation
AKRacing is the official gaming chair sponsor of PlayerUnknown's Battlegrounds (PUBG) Global Invitational North American Qualifiers.
AKRacing at PUBG Global Invitation
AKRacing is the official gaming chair sponsor of PlayerUnknown's Battlegrounds (PUBG) Global Invitational North American Qualifiers.
AKRacing at eMLS Cup PAX East 2018
AKRacing is the official gaming chair sponsor of PAX and the gaming chair of choice of eMLS Cup players.
AKRacing at eMLS Cup PAX East 2018
AKRacing is the official gaming chair sponsor of PAX and the gaming chair of choice of eMLS Cup players.
AKRacing at PAX West 2017
AKRacing is the official gaming chair sponsor of PAX (East, South and West) in 2017 and 2018.
AKRacing at NHL Gaming World Championship
AKRacing is the official gaming chair sponsor of the NHL Gaming World Championship in Europe, Canada and USA.
AKRacing at NHL Gaming World Championship
AKRacing is the official gaming chair sponsor of the NHL Gaming World Championship in Europe, Canada and USA.
AKRacing at Intel Extreme Masters
AKRacing collaborated with MSI at Intel Extreme Masters in Australia.
AKRacing at Intel Extreme Masters
AKRacing collaborated with MSI at Intel Extreme Masters in Australia.
AKRacing at eMLS League Series One Los Angeles 2019
AKRacing custom eMLS Gaming Chairs at all eMLS League Series events.