Non-Latex Rubber Bands with Antimicrobial Protection

Alliance Antimicrobial Non-Latex Rubber Bands are a healthy choice for use in latex-free environments at home or in the workplaces, especially in medical facilities. Unlike common office rubber bands, the antimicrobial protection embedded in these rubber bands resists bacteria, mold and fungi, which can cause elastics to deteriorate faster. The synthetic rubber formulation of these bands also won't cause reactions in those with latex allergies, making them a safe choice when latex sensitivity is a concern. The soft stretch design means the elastics are easy to manipulate, which can help in reducing symptoms related to carpal tunnel syndrome from repetitive actions.


  • Made with a non-latex synthetic rubber compound with antimicrobial ​ protection
  • Size #33 (3 1/2" x 1/8")​
  • 1/4 lb box contains approx. 180 bands​
  • Color: Cyan Blue

Antimicrobial Elastic Bands Offer Greater Protection and Durability

Package Foods Safely

Prepared food that's been in contact with latex can cause allergic reactions in latex-sensitive individuals. Instead, use these antimicrobial non-latex rubber bands to secure packaged foods or keep items bundled and organized in the fridge.

Prevent Latex Reactions in Medical Offices

Patients and visitors to medical offices shouldn't have to worry about experiencing allergic reactions or exposure to bacteria. These antimicrobial non-latex elastics help prevent issues with latex sensitivity and inhibit the spread of germs, mold and fungi. Bundle medical utensils or secure plastic coverings on equipment using these bands.

Protect Against Latex Reactions at Work

Latex rubber bands can be found all over the workplace. Make your office environment comfortable and safe for all staff members by using antimicrobial non-latex elastics that won't trigger reactions in latex-sensitive individuals while also guarding against the transfer of germs.

Provide a Safe School Environment

Prevent latex exposure and combat the spread of bacteria by using antimicrobial non-latex rubber bands in school offices and in classrooms. Their bright blue color clearly distinguishes these elastics from regular office rubber bands and those without antimicrobial protection.

Alliance Rubber Company is a family-owned business with humble beginnings that has grown into a thriving American success story. Since 1923, Alliance Rubber has proudly produced rubber bands for use in the home and workplace. Continuing to manufacture its products in the USA, enables Alliance to provide high quality products, fast service and fresh stock that is built to last. Alliance Rubber, a women owned company, manufactures bands that ‘Hold Your World Together’.​​​​​​