For ten years, AMD Socket AM4 has been at the center of millions of gaming and PC builds around the world. It delivered smooth gaming and dependable performance, all while making upgrades simple and accessible.
From its first launch to today, AM4 has continued to evolve through multiple processor generations without requiring a new motherboard, giving PC builders a platform they could trust and grow with over time.
Over the past decade, AMD Socket AM4 has grown into one of the most widely adopted desktop platforms in the PC community.
• 10 years of powering PC enthusiasts around the world
• 5 generations of CPU Architectures supported on a single platform
• 125+ AMD Ryzen™ processors launched for Socket AM4
• 500+ Socket AM4 motherboard models, giving builders broad choice and flexibility
These milestones reflect AMD’s long standing commitment to platform longevity and upgrade flexibility.
A huge thank you to our motherboard partners—ASRock, ASUS, BIOSTAR, GIGABYTE, MSI, and SAPPHIRE—for helping make Socket AM4 a platform PC builders could count on year after year.
The AMD Ryzen™ 7 5800X3D Processor stands as the ultimate gaming processor for DDR4 platforms, showcasing how far the AM4 platform could be taken for gamers delivering an average of 10% more fps than the 14900K when using DDR4-3600 MHz memory, and on a platform that has supported upgrades over 6 years longer. 1,2
Built on the proven Ryzen™ 5000 Series with AMD “Zen 3” architecture cores and 7nm process technology, it introduced 1st Gen AMD 3D V Cache™ technology to desktop gaming and raised expectations for performance on an established platform.
As the first gaming processor to feature 3D stacked cache, the Ryzen 7 5800X3D delivers a massive 96MB of L3 cache to help boost gaming performance and responsiveness across a wide range of titles. The result is smoother gameplay, higher framerates, and lower latency, making the Ryzen 7 5800X3D one of the most celebrated gaming processors ever released on Socket AM4.
One of the defining strengths of AMD Socket AM4 has always been its ability to deliver meaningful performance upgrades without requiring a full system rebuild.
Designed to drop directly into existing AM4 systems with supported motherboards, the Ryzen 7 5800X3D processor allows users to unlock a new level of gaming performance while keeping their motherboard, memory, storage, and cooling intact. It is a straightforward path to extending the life of an already trusted system.
For those gamers who are looking for the maximum uplift through an in-socket upgrade on their existing motherboard, the Ryzen™ 7 5800X3D processor can deliver over 2X higher gaming performance FPS across a range of games compared to Ryzen™ 7 2700X, and over 40 percent versus Ryzen™ 7 3700X when paired with a high-end graphics card. 3,4
Every Ryzen™ 7 5800X3D processor comes bundled with a Carbice® IcePad™ thermal pad, adding extra value for gamers upgrading within the AM4 platform.
While traditional thermal paste can perform well initially, many paste suppliers recommend repasting over time to help maintain optimal performance. Carbice® IcePad™ is designed to settle quickly and deliver more consistent thermal performance across extended use, without the mess or upkeep of reapplication.
This is another way AMD helps AM4 users extend system life with fewer hassles and dependable long‑term reliability.
AM4 sets the standard. AM5 carries it forward.
AMD Socket AM5 brings forward the same focus on long-term value, forward compatibility, and meaningful upgrades over time. Designed to support new performance technologies and evolving workload demands, AM5 continues AMD’s commitment to giving builders a platform that can grow with them.
Processors like the Ryzen™ 7 7700X3D showcase how AMD is expanding the breadth of options across the AM5 stack, giving gamers and builders more choices — whether they’re upgrading within the platform or making the move to AM5 for the first time.
From its debut to its tenth year, AMD Socket AM4 has redefined what long-term PC platforms can be.
With the return of the Ryzen™ 7 5800X3D processor, AMD celebrates not just a milestone but a philosophy: build a platform that lasts and give users meaningful reasons to keep upgrading.
And as AM5 carries that philosophy forward, the story of long-term platform innovation at AMD continues.
Check out the AMD Gaming Computex Announcements on YouTube!