Acer Chromebook Plus Enterprise Spin 714

Lift. Flip. Spin. Plus More Power

Acer Chromebook Plus Spin Enterprise 714 (CPE794-1N)
Acer Chromebook Plus Spin Enterprise 714 (CPE794-1N)
Powered by the latest Intel ® Core™ Ultra Processors 1–the Acer Chromebook Plus Spin 714 is the embodiment of power and portability. A premium thin and light 2-in-1 convertible Acer Chromebook for work in office or on-the-go.
300x150-1-36
300x150-2-37
Acer_Chromebook_plus_E_Spin 714_KSP07
300x150-3-37
300x150-4-37

Your Work, Your Way

Carry your work around in style with an 18.05mm1 thin and 1.46kg1 light 2-in-1 convertible Acer Chromebook made with durable aluminum chassis.

acer_chromebook_plus_e_spin 714_ksp01
Acer_Chromebook_plus_E_Spin 714_KSP01-1_1440x800
Precision with every stroke

Draw with precision using the tilt and pressure sensitive Active Stylus1. Store and charge your stylus in the stylus garage without worrying about losing it.

Acer_Chromebook_plus_E_Spin 714_KSP01-2_1440x800
Stay productive day and night.

Work through the night on a precision keyboard with backlight1.

Acer_Chromebook_plus_E_Spin 714_KSP01-3_1440x800
Military-Grade Durability

Made to be durable and reliable-this Acer Chromebook undergoes stringent test procedures, meeting MIL-STD 810H6 standards to withstand everyday wear and tear.

Do more than you thought you could

Powered with Intel® Core™ Ultra processor1 this Chromebook Plus offers more than just a performance score, advancing real-world computing and delivering efficient multi-tasking.

  • Up to 16 GB

    LPDDR5 Memory1

  • Up to 512 GB

    SSD Storage1

  • Titan C2

    Security Chip

Acer_Chromebook_plus_E_Spin 714_KSP02-01_1440x800
Stay productive offline.

File Sync, available with Acer Chromebook Plus, automatically syncs files to File Manager, so Google Docs, Sheets, and Slides are always accessible — even when offline3.

Acer_Chromebook_plus_E_Spin 714_KSP03-01
Built-in video call control tools

Automatically enhance clarity and lighting, cancel noise, and blur backgrounds.

Work Smarter, not Harder

With 2X the power, speed, memory, and storage of other devices, and a high-definition camera and display, your people are empowered to do their best work2.

acer_chromebook_plus_e_spin 714_ksp03
Acer_Chromebook_plus_E_Spin 714_KSP03-1_1440x800
Proactive security that reduces your attack surface

A secure by design OS that protects your people from security breaches, and your bottom-line profitability from costly attacks.

Acer_Chromebook_plus_E_Spin 714_KSP03-02_1440x800
Software and hardware features to activate worker productivity

Our modern, cloud-first OS coupled with 2X the power, speed, memory, and storage of our devices, empowers your people to do their best work, whether they’re in-office, remote – or anywhere in between

Acer_Chromebook_plus_E_Spin 714_KSP03-03_1440x800
Get more done at a lower cost

Reduce your cost of ownership with devices that have a 245% ROI over three years8.

A Touch of Magic

Witness magic on the 14” WUXGA (1920 x 1200)1 Antimicrobial Gorilla Glass display with touch. See more on the 16:10 narrow bezel display and dive into a whole new visual and audio experience with DTS® audio.

 

86.5%

Screen-to-body ratio1

 

350 nits

Brightness1

 

100% sRGB

Color1

acer_chromebook_plus_e_spin 714_ksp04

Crystal Clear Calls

This Acer Chromebook Plus has a 1440p QHD webcam1 with HDR and built-in AI-powered video call tools that enhance clarity and lighting to look your best on any video call app.

acer_chromebook_plus_e_spin 714_ksp05
acer_chromebook_plus_e_spin 714_ksp05-1
Acer TNR Solution

Detects, diagnoses, and improves image quality in low-light conditions.

acer_chromebook_plus_e_spin 714_ksp05-2
Facial Auto-exposure

Automatically adjust the image exposure based on the lighting conditions of your face.

Connect with Ease

With fast WiFi 6E1 and Bluetooth 5.21 connectivity, connect to all your favorite accessories and devices.

 

Thunderbolt 4

Type C

 

USB 3.2 Gen 1

Type A

 

2.0

HDMI

acer_chromebook_plus_e_spin 714_ksp06

ChromeOS

ChromeOS is a cloud-first operating system that provides employees with a modern experience and devices that stay fast, have built-in security, deploy quickly, and reduce the total cost of ownership.

Acer_Chromebook_plus_E_Spin 714_KSP07
acer_chromebook_plus_e_spin 714_ksp07-1_1440x800
Chrome Enterprise Upgrade

Chrome Enterprise Upgrade unlocks the built-in business capabilities of ChromeOS devices for IT to secure, orchestrate, and power the cloud workforce, with 24/7 IT admin support.

acer_chromebook_plus_e_spin 714_ksp07-2_1440x800
Zero-Touch Enrollment

Featuring zero-touch enrollment, IT departments will be able to drop ship ChromeOS devices that will be automatically enrolled into enterprise administration as soon as the user connects to the internet.

Sustainability

Featuring recycled materials, sustainable packaging, an energy-efficient design, and EPEAT registration7, this Acer Chromebook Plus embodies the spirit of our Earthion initiative to reduce waste across the lifetime of the device.

Acer_Chromebook_plus_E_Spin 714_KSP08-0
acer chromebook plus_e_spin 714_ksp08-1_720x400​
Less Plastic Waste in the Ocean

We use recycled ocean-bound plastic in the OceanGlass™ touchpad of this Acer Chromebook Plus. The touchpad gives you a sleek, glass-like tactile feel as your fingers scroll across its surface

acer chromebook plus_e_spin 714_ksp08-2_720x400
Conserve Natural Resources

Our molded pulp packaging uses recycled paper, cardboard, and other natural fibers, offering greater sustainability benefits than traditional plastic and Styrofoam packaging.

1. Specifications of this device may vary depending on model and/or region.
2. When compared to top selling Chromebooks from July 2022 to Dec 2022.
3. You must be connected to the internet to set up this feature. Download required. Must have available storage space in Drive.
4. Additional functionality available with Microsoft 365 ® subscription. Microsoft, Excel and PowerPoint are registered trademarks of Microsoft Corporation. 
5. Battery life may vary based on device and upon usage and other conditions. 
6. MIL-STD 810G/H is a testing protocol conducted in controlled settings and does not guarantee future performance in all situations. Do not attempt to simulate these tests, as damage resulting from this will not be covered by Acer's standard warranty
7. EPEAT ® registration varies by country. See http://www.epeat.net/ for registration status for each country.
8. IDC Business Value Snapshot, sponsored by Google ChromeOS, The Business Value of ChromeOS, doc #US50055223, January 2023