USB 3.2 (10Gb/s) Bus-Powered Portable NVMe SSD
The OWC Envoy Pro Elektron is the fastest, toughest mini USB-C SSD in the galaxy. This crushproof, dustproof, and waterproof drive pushes the bandwidth of the USB-C interface to the max so you can edit and save anywhere, anytime. We aren’t the only ones singing its praises. The OWC Envoy Pro Elektron won the Gamesradar+ Editor’s Choice Award and took the Recommended category at Windows Central. The OWC Envoy Pro Elektron was a 2021 honoree at CES Innovation Awards and was reader-nominated for the 2020 Future Tech Awards. Experience for yourself why critics around the world are raving about the OWC Envoy Pro Elektron – the highly compatible, pocket-sized powerhouse that fits in the palm of your hand.
Since the earliest days of portable computing, “make it smaller, faster, lighter, and rugged,” has been a common goal. Pocket-sized, crushproof, dustproof, and waterproof, the OWC Envoy Pro Elektron puts all of your personal and work files in the palm of your hand while pushing the bandwidth of the USB-C (10Gbps) interface to the max so you can edit and save wherever, whenever with virtually any Mac or PC.
With up to 2x faster performance than other portable SSDs, you'll feel the speed every time you save, edit, or backup files
Advanced NVMe technology delivers superior performance coupled with built-in OWC reliability
Plug and play with Macs, PCs, iPad Pros, Chromebooks, and Android tablets from the last decade, current models, and well into the future
The go anywhere storage solution that’s half the size of a smartphone
Crushproof, dustproof and waterproof IP67 rated
At-a-glance LED for confirmation of power and activity status
Install an OS or work with alternate OSes. Startup and launch apps in mere seconds
Connect universally to any USB-C or Thunderbolt computer or device.
Heat-dissipating, aircraft-grade aluminum housing for silent, throttle-free, breakneck performance
Edit large format video footage in the field. Take your favorite games and music with you to play anywhere. Back up that work or classroom project. Whatever your data storage need, the OWC Envoy Pro Elektron lets you do it all up to twice as fast as other portable SSDs in a reliably rugged solution that’s half the size of a smartphone.
Big theoretical performance numbers are certainly eye-catching, but they rarely reflect real-world performance. That’s why we take the extra time to run our storage solutions through intensive performance testing. Truthfully listing real-word test results demonstrates “The OWC Difference,” and our commitment to your complete satisfaction that the OWC Envoy Pro Elektron will handle your most demanding needs.
It’s easy to get beguiled by the sleek, silent, and cool running aircraft-grade aluminum housing. More than just a pretty face, the OWC Envoy Pro Elektron is IP67 rated so you can work in the dirtiest and wettest environments. And if you happen to drop this hyper-portable drive onto a driveway or parking lot, the crushproof Envoy Pro Elektron can be rolled over multiple times without damage to your precious data inside.
Work faster when you pair OWC Envoy Pro Elektron (480GB, 1TB, and 2TB models) with your USB-C equipped Blackmagic, Fujifilm, and Panasonic camera. By recording all formats and resolutions directly to Envoy Pro Elektron, you’re automatically ingesting. Now instead of needing a costly card reader to offload, just start editing off Envoy Pro Elektron for a faster turnaround.
All the features and “technospeak” of an external drive don’t mean a thing without real-world examples of the files you know. Let’s break it down and see how much space a single terabyte offers.
For every 1TB of OWC Envoy Pro Elektron SSD capacity, you can store: