Automatically disinfect your workstation device accessories — like your keyboard, mouse, or just about any device — reducing the need for manual intervention, cleaning, or touching.
As companies and individuals look for effective solutions to maintain a cleaner work environment, the Targus UV-C LED Disinfection Light is an essential no-touch solution to help reduce pathogens on device surfaces. Sleek, modern, and lightweight, the Disinfection Light is designed to stand between your keyboard and monitor on the desktop to automatically disinfect the surfaces of keyboards, mice, and other items within the disinfection range¹. It even has a nook to hold your smartphone during the disinfection cycle.
Incorporating state-of-the-art UV-C LED and automation technology, the AC-powered light turns on and runs for 5 minutes, every hour, to break down the DNA of microorganisms. Regular use is effective at eliminating harmful pathogenic microorganisms on device surfaces and complements cleaning regimens and hygiene safety measures.
When the disinfection cycle begins, it emits a purple ambient light, indicating the Disinfection Light is in use. There is a built-in auto shut-off safety feature that utilizes motion sensors. Should any motion be detected within the safety zone², outside of the active cleaning area, or if the device senses any activity within the safety zone, the UV-C LEDs will be automatically disabled. After 5 minutes of inactivity, the Light will resume its disinfection cycle.
¹ Disinfection area is estimated at 10” deep by 26” wide.
² Safety zone is estimated at 18” beyond the disinfection area.
³ The CES Innovation Awards are based upon descriptive materials submitted to the judges. CTA did not verify the accuracy of any submission or of any claims made and did not test the item to which the award was given.
UV-C light is a proven disinfection method designed to effectively kill or inactivate pathogenic microorganisms. Third Party laboratory testing verified efficacy against Flu Virus (H1N1 Influenza), Staph (Staphylococcus aureus) Bacteria, Pneumonia (Klebsiella pneumoniae) Bacteria, and MRSA (methicillin-resistant Staphylococcus aureus) Bacteria. The Targus UV-C LED Disinfection Light runs for 5 minutes, every hour, to clean the active disinfection area. When the disinfection cycle begins, the light emits a purple ambient hue, indicating that it is in use.
AC-powered, the disinfecting occurs automatically, so there is no manual cleaning schedule to maintain. It’s the perfect, low maintenance, automated disinfection solution for individual workstations to eliminate pathogenic microorganisms on high-touch surfaces. Manual cleaning, however, can be initiated with the press of a button, allowing 15 seconds for the individual to leave the active area.
Utilizing motion sensors, the UV-C LED Disinfection Light automatically shuts off the system if movement is detected within the safety zone or directly outside of the active cleaning area. After 5 minutes of inactivity, the light will resume its disinfection cycle.
The Targus UV-C LED Disinfection Light is a CES® 2021 Innovation Awards Honoree³. This UV-C LED Disinfection Light delivers the perfect low maintenance, automated disinfection solution for individual workstations to eliminate most pathogenic microorganisms on critical high-touch surfaces of items like keyboards, mice, and tablets.