The wireless desktop set – Ergonomic and quiet working at its best
Want to play it safe? A desktop set that will last, looks great, and is a joy to use? Here it is. With the CHERRY STREAM DESKTOP you know exactly what you are going to get. It is both new and proven at the same time. After many product generations, the CHERRY STREAM KEYBOARD has been developed to absolute perfection. The STREAM, revised in 2019, is the best STREAM ever — and it is now also available as a wireless version with a matching partner of the same caliber: the STREAM mouse.
With this new wireless duo you can’t go wrong. The pair complement each other in both design and technology. We didn't just throw a mouse onto the side of the STREAM keyboard, but developed one that fits the aesthetic and feels great with it. It looks just as good and is just as quiet when clicked as the STREAM keyboard. And they're both incredibly reliable, durable and built to last. Whether in the office or when working from home. You see, this is not just any duo, but one with a coherent concept.
What makes a keyboard a really good keyboard? When it not only looks good, but also feels good when writing and typing at speed: very little noise, precise pressure points, the very best typing experience. Thanks to the high-quality and particularly precise CHERRY SX scissor technology, the STREAM keyboard offers you a new typing experience.
All good things come in sixes! That's because the STREAM mouse has not three, but six buttons — and a 3-position adjustable DPI switch. Silent switches are built in under the buttons. They are chosen so that the Silent click is particularly quiet. To ensure that the mouse is as sophisticated as its keyboard partner, its ergonomics have also been meticulously tested. Large or small, right or left — the mouse fits in all hands.
Thanks to CHERRY’s high quality standards, the STREAM mouse and keyboard deliver the reliability you are used to. In addition to their high degree of design and technology, they are also top quality. The integrated metal plate and the stable support feet ensure that the keyboard stays firmly in position on your table, and does not slip with every touch. Similarly, the mouse has an ideal weight: It lies light and secure in the hand and moves smoothly and comfortably. This duo will be a real joy to work with for a long time, as they are durable and high quality products.
The use of high-quality scissor mechanisms with a low key stroke ensures an ideal typing experience. Status LEDs integrated directly in each key provide information on whether the CAPS LOCK, SCROLL and NUM keys are activated. In addition, these keys flash to warn that the battery charging status is low.
With the new CHERRY STREAM DESKTOP, your fingers can easily get to work. Flat keys, precise touch, faster typing — and the chance to get more done. The keyboard is perfect for those who type a lot and who highly value comfort when working.
CHERRY STREAM DESKTOP COMFORT
Both wireless. Both ergonomic. Both incredibly quiet. The CHERRY STREAM DESKTOP COMFORT is a perfect combination. The new member of our STREAM family is a set comprising a wireless keyboard and a wireless, ergonomic right-handed mouse. The high-quality desktop set can be connected easily and wirelessly using a 2.4 GHz USB receiver. Due to the extremely quiet keystroke and the near-silent mouse buttons, this ergonomic keyboard and mouse set is also perfect for those who like to work in a quiet environment. Thanks to the rubberized thumb pad, your hand assumes a an ideal position on the elegant right-handed mouse, enabling you to click in a relaxed manner throughout your everyday tasks.
The keyboard’s shape is based on our best selling STREAM KEYBOARD, which has sold in millions and gained plenty of fans all over the world. It is a flat, yet stable keyboard thanks to its internal integrated metal plate. In addition, it has a total of eight rubber pads on the underside as well as two rubberized, robust fold-out feet, which prevent slipping even during the busiest periods.
With its ergonomic shape, the right-handed mouse is perfect for use by medium or larger hands. It has a comfortable thumb rest with a cool Voronoi design which not only looks good, but also encourages a relaxed hand position. The 6-button mouse has a metal scroll wheel with a high-quality feel and delivers precise control during scrolling. The large pads on the underside make a real difference for ease of use: the mouse slides over the desktop effortlessly.
CHERRY SX scissor technology is the unmistakable trademark of our STREAM line. It means that the flat CHERRY STREAM DESKTOP COMFORT keyboard delivers the familiar unbeatable typing experience as well as precise and, above all, near-silent keystrokes. The right-handed mouse has just as much to offer as the keyboard. It also features quiet buttons which operate in almost complete silence. The four-stage adjustable sensor with up to 4000 DPI enables precise control of the mouse pointer to make work even more productive. The ergonomic keyboard and mouse set are perfect partners.
The CHERRY STREAM DESKTOP COMFORT is easy to connect with its extra small nano-USB 2.4 GHz receiver. Simply place it in the USB port of your device and the ergonomic mouse and keyboard set will function wirelessly and flexibly within a range of 10 m. You can also store the receiver magnetically in the mouse if you have to transport the set. Secure data transfer is ensured by the AES-128 encryption.
The keyboard of the CHERRY STREAM DESKTOP COMFORT bundle ensures you have everything under control. The 10 additional keys deliver fast access to the most frequently used office and multimedia functions. The convenient side buttons on the mouse enable you to navigate back and forth in an Internet browser with ease. Our free CHERRY KEYS software enables you to assign both the function keys of the keyboard and the side mouse buttons so that they meet your requirements. Incredibly practical: The CAPS LOCK, NUM and SCROLL button status LEDs on the keyboard flash to indicate when it is time to change the battery. The same applies to the DPI switch on the mouse - it also flashes when a new battery is required. The ergonomic keyboard and mouse set has a battery life of up to 36 months. Moreover, you can simply switch off both the mouse and keyboard when they are not in use.
Our CHERRY STREAM DESKTOP COMFORT has GS approval ("Tested Safety"). This is a globally recognized seal that ensures that a product complies with all relevant European directives and regulations relating to the health and safety. The keyboard has also been awarded the "Blue Angel" ecolabel, a German award for particularly sustainable products. Finally, the ergonomic keyboard and mouse set comes in completely plastic-free packaging.
Our STREAM DESKTOP COMFORT is not only a perfect match in appearance, but also in terms of technology and ergonomics. A durable, innovative product which is easy to use and will soon become an essential tool in your everyday working life. See for yourself and type/click through the day ergonomically, wirelessly and quietly with this mouse and keyboard set.