While our base model Gemini is great for everyday content creators, you are worlds beyond ordinary. Your workflow is at the extreme edge of resolutions, codecs, and framerates. We understand your need to push into an ‘other world’ of capability, and pros like you are the reason we created the Gemini Ultra.
Powered by up to six NVMe SSDs, you’ll have the horsepower to handle the most demanding photography, video, and editing tasks you face. Edit ultra-high resolution files on the fly, ingest several media cards in parallel and render dailies without a hitch, and rip through 8K footage with up to 2381MB/s real world speed. 1
Beyond performance, with Gemini Ultra’s seven connectivity ports, you will experience an incredible level of versatility. Use your favorite accessories and charge small mobile devices via two USB ports. Daisy chains up to five Thunderbolt devices so that you can create additional backups. Offload media cards faster and easier with the frontside UHS-II slot or external card readers via Thunderbolt or USB-C. Transfer files and work up to 2.5x faster over wired networks and enjoy increased productivity when working with NAS devices with 2.5Gb/s Ethernet. Add an external monitor with up to 8K resolution via HDMI.
Make your dream of becoming an editing powerhouse a reality by utilizing the performance of NVMe SSDs. With dual drives preset in SoftRAID RAID 0, you’ll have 1446MB/s 3 of bandwidth to handle demanding media workflows such as 8K video and 6K multicam sequences using advanced 10 bit and 12 bit codecs, high framerate footage, and ultra-high resolution RAW pictures. Plus, you’ll have all the advanced drive health monitoring benefits of SoftRAID so you can work worry-free. You can also use SoftRAID to change to RAID 1 data protection with speeds up to 721MB/s.
Level up to the ultimate production grade workflow storage and docking convenience solution on the market. This dual drive model adds higher capacity and RAID configuration possibilities – like RAID 0 for speed or RAID 5 for data protection – to empower you with advanced performance. And SoftRAID is there helping you manage it all easily.
With multi-drive media dumps, controllers, A/V outputs, and a mess of device cables, it can be hard enough to find space for your notebook let alone room to work. Cure your clutter woes by reclaiming your workspace with Gemini Ultra’s centralized design. The latest technology advances in storage, ethernet speed, connection speeds, and display support deliver the professional results your work demands while neatly consolidating all your devices.
OWC Innergize™ is the first stage of the Capture to Completion™ ecosystem of OWC products designed to seamlessly propel professional photographers, videographers, and content creators to the highest level of workflow performance and reliability. This OWC custom-designed app is a complete health, performance, and field upgrade management tool when using OWC Atlas memory cards with OWC Atlas readers and reader equipped products.
Over time and use cycles, flash memory does wear out. Innergize verifies and reports the percentage of use life remaining. Now you can work with full confidence your OWC flash memory product will deliver the reliability you can trust.
Writes, deletes, and formatting all take their toll on memory cards. Innergize cleans and restores the flash memory performance of OWC memory cards so you can get the best results on every use.
When new cameras or firmware updates to existing cameras are introduced, they may not work properly with flash memory cards and drives. Innergize gives OWC memory card users the ability to quickly upgrade their firmware in the field for full compatibility, additional performance enhancements, and bug fixes for optimal reliability.
SoftRAID is the world’s fastest and most flexible application to configure, maintain, and protect your RAID volumes on Mac and PC. OWC enclosures include 3 Years of SoftRAID Premium.
M1 Macs require macOS 11.3 or later. SoftRAID is licensed per computer.
Safely disconnect multiple drives in a single click. OWC Dock Ejector was designed by OWC hardware and software engineers to ensure all data is written before disconnection, saving time and protecting against data loss. It makes losing your hard-earned work a thing of the past.
Active workspaces expose gear to bumps, shoves, or even the random tail wag from a pet. OWC ClingOn custom cable stabilizers (sold separately) screw into the OWC Dock or OWC Drive housing to reduce – if not completely eliminate – cable strain on Thunderbolt and USB-C connections so you can work with confidence even in the highest traffic environments.
OWC Gemini comes with a certified 0.7M OWC Thunderbolt Cable. But if your workflow demands a different length to make the connection, OWC Thunderbolt (USB-C) Cables are the perfect choice.