World’s FASTEST and HIGHEST Capacity PCIe SSD

  • Revolutionary: The fastest drive available for 2019 Mac Pro or Windows computers
  • Mind-blowing Performance: Up to 12,000MB/s real world PCIe Gen 3 speeds today
  • Future Upgradeable: Beyond 26,000MB/s speed with PCIe Gen 4 systems
  • Massive Space: Add up to eight SSDs for jaw-dropping storage capacity
  • Bleeding Edge Design: Utilizes the full bandwidth of the latest PCIe technology
  • Includes SoftRAID: robust software for creating, monitoring, and managing advanced RAID sets
  • Advanced RAID Capabilities: Supports multiple RAID levels and RAID sets for maximum flexibility
  • Quietly Cool: Highly efficient and quiet heat-dissipating design for consistent peak performance
  • Plug and Play: No drivers needed

Astonishingly, Mind-Blowingly Holy Cow Fast

Whether it leaves you speechless in amazement or uttering colorful phrases, the Accelsior 8M2 can be summed up in one definitive sentence: It’s the fastest, highest capacity PCIe SSD in the galaxy. This beast destroys performance barriers and every PCIe SSD on the market today. So much so that we considered naming it the Annihil8r! We continuously push the boundaries of SSD capabilities so you can realize your true potential. With the Accelsior 8M2, we’re taking you beyond your wildest dreams and into the most demanding applications imaginable with certified reliability. From M&E postproduction, to real-time AI, to huge dataset climate research… you now have the power to confidently reach higher.

Obliterates Workflow Bottlenecks

As storage performance innovators, we know that bottlenecks cramp your style. The Accelsior 8M2 was purposely created to be the fastest drive you can use in any workflow. With eight on-board NVMe SSDs and speeds up to 12,000MB/s on the PCIe Gen 3 equipped 2019 Mac Pro, video editors have the real world speed for sustaining the most demanding VFX, color, and high-end video editing including seamless playback of:

  • 16 streams of 8K ProRes444 in Final Cut Pro X
  • 8 streams of 12K ProRes444 in Final Cut Pro X
  • 9 streams of 4K 16bit EXR in DaVinci Resolve

Now you have the overhead to go faster, process more, and save almost limitlessly.

Ultra-Reliable Design

Creating the fastest PCIe SSD meant combining bold engineering with the latest technology. Each of the Accelsior 8M2’s eight NVMe SSDs run at their full x4 lanes of PCIe Gen 3 data throughput. All that insanely fast speed is pumped through a full PCIe x16 lane architecture. And to ensure Accelsior 8M2 keeps running at peak speed for the long haul, there’s a quiet cooling fan in the aircraft grade aluminum heat sink. And when PCIe Gen 4 SSDs and systems become more widely available, it's an easy upgrade to experience speeds over 26,000MB/s on a PCIe Gen 4 machine, No compromises. No surrender. Just the ultra-reliable performance that Mac and PC users have come to depend on from OWC storage solutions.

Crushes I/O Intensive Apps

When work requires your storage device to deliver maximum IOPS (Inputs/Outputs Per Second) performance, the Accelsior 8M2 crushes data crunching tasks in a fraction of the time. Cloud applications, climate research, virtualization apps, you name it…the Accelsior 8M2 accelerates them all so you can work more efficiently.

When Survival Depends on Reliable Performance

Government agencies, companies, and institutions need the ability to reliably access and quickly analyze enormous data files to make decisions. The Accelsior 8M2 is ideal for “big data” geospatial apps used by emergency management organizations to process real-time conditions, such as natural disasters like a fire or flood. Officials making life-saving decisions can count on the Accelsior 8M2 to deliver actionable data in extreme situations where every second matters.

Reduces Timelines and Project Budgets

Whether you’re a Media and Entertainment production pro or a transportation logistics wizard, there’s one ever-present formula that affects your success: Time = Money There’s a priceless benefit in knowing you can work as fast as possible. Every microsecond saved adds up to money saved for your company. Case in point, a multiple Academy Awards™ winning film production company is currently using the best available storage technology, but still has workflow limits.Here are some of the company’s problems that could be solved by implementing the Accelsior 8M2:

  • Not enough capacity to store multiple reels, so they have to shuttle reel media between the main ingest drive and slower external storage devices.
  • The time-consuming process of accessing a finished reel on external drives.
  • Struggling with drive space-saving methods like flattening project layers, which requires re-rendering layers you’re working in.
  • Not enough speed to view real-time playback. Playback must be viewed in several different modes to determine effects of filters and adjustments.
  • Not enough speed to ensure smooth playback of industry’s emerging 8K and 10K 16bit film.

By eliminating the need to remove a reel and renders from their current storage platform, this company can shave up to two days from their production schedule. The Accelsior 8M2 could reduce production costs for this company with typical production projects of 10 reels of film by an estimated $8,000 per project , making this revolutionary SSD a seriously smart investment.