OWC Atlas Ultra CFexpress

High-performance, highest quality memory card for the most demanding video recording uses of professional filmmakers and continuous burst mode shooting by advanced photographers.

The Fastest, Most Reliable CFexpress Card

When you need the fastest, most reliable CFexpress card, the Atlas Ultra CFexpress is ready to take you to the edge. With incredibly high minimum sustained write speeds up to 1500MB/s, this is the perfect media card for pro filmmakers or extreme action photographers to unleash their cameras capabilities.

Professional filmmakers can capture amazingly life-like 8K RAW video in slow-motion with cinema cameras like the Nikon Z9, Canon R5C, and RED V-Raptor. As a testament to its quality, the Atlas Ultra CFexpress is one of only several media cards that meets RED Digital Cinema’s stringent test standards and has been officially approved for use with their RED V-Raptor Cinema camera.

Truth in Numbers

Big theoretical performance numbers are certainly eye-catchers, but they are misleading when your workflow requires real-world speed. That’s why we take the extra time to run OWC flash storage solutions through intensive performance testing, and we share our test setup and parameters. Truthfully listing Atlas Ultra CFexpress cards for reliable peak performance up to 3000MB/s write, 3650MB/s read, and up to 1500MB/s sustained write speed defines our commitment to the “OWC Difference,” which ensures these CFexpress Type B cards will deliver the performance you are counting on.

Maximum Sequential and Sustained Read/Write Performances delivered by OWC Atlas Ultra CFexpress 4.0 Cards

Details matter when it comes to making an investment into a memory card for your camera. That is why OWC Atlas Ultra CFexpress 4.0 cards leverage the CFA 4.0 specification that is backward compatible with CFA 2.0 (i.e. PCIe Gen3) cameras and readers of today, and forward compatible with CFA 4.0 (i.e. PCIe Gen4) cameras and readers of the future delivering the highest performance that you deserve.

After intensive stress tests with multiple full capacity cycles, the Atlas FXR reader still delivers consistent sustained 1400MB/s read and 1200MB/s write performance from a 2TB Atlas Ultra CFexpress card while maintaining a safe temperature.

 

Innergize Your Workflow with Highest Performance and Reliability

OWC Innergize™ is the first stage of the Capture to Completion™ ecosystem of OWC products designed to seamlessly propel professional photographers, videographers, and content creators to the highest level of workflow performance and reliability. This OWC custom-designed app is a complete health, performance, and field upgrade management tool when using OWC Atlas memory cards with OWC Atlas readers and reader equipped products.

                       Work with Maximum Confidence and Reliability

Health

Over time and use cycles, flash memory does wear out. Innergize verifies and reports the percentage of use life remaining. Now you can work with full confidence your OWC flash memory product will deliver the reliability you can trust.

Sanitize

Writes, deletes, and formatting all take their toll on memory cards. Innergize cleans and restores the flash memory performance of OWC memory cards so you can get the best results on every use.

Field Upgrade

When new cameras or firmware updates to existing cameras are introduced, they may not work properly with flash memory cards and drives. Innergize gives OWC memory card users the ability to quickly upgrade their firmware in the field for full compatibility, additional performance enhancements, and bug fixes for optimal reliability.