OWC Atlas Pro CFexpress

Cost-effective, highest quality memory card for the most demanding needs of professional photographers and the most common use cases of professional filmmakers

Awesome Professional Performance Made Affordable

When you want a CFexpress Type B memory card that checks all the boxes for all the most common professional workflow needs, Atlas Pro CFexpress is your cost-effective choice. You’ll enjoy awesome performance for the most demanding photo projects including action sports and wildlife photos. Capture up to 6K high bitrate video. Whether you’re a photographer using a firmware updated XQD camera and only need modest storage or are a filmmaker using the latest camera, there’s an Atlas Pro CFexpress card in the optimal capacity for your specific need.

 Truth in Numbers

Big theoretical performance numbers are certainly eye-catchers, but they are misleading when your workflow requires real-world speed. That’s why we take the extra time to run OWC flash storage solutions through intensive performance testing, and we share our test setup and parameters. Truthfully listing Atlas Pro CFexpress cards for reliable peak performance up to 3000MB/s write, 3650MB/s read, and up to 800MB/s sustained write speed defines our commitment to the “OWC Difference,” which ensures these CFexpress Type B cards will deliver the performance you are counting on.

Maximum Sequential and Sustained Read/Write Performances Delivered by OWC Atlas Pro CFexpress 4.0 Cards

Details matter when it comes to making an investment into a memory card for your camera. That is why OWC Atlas Pro CFexpress 4.0 cards leverage the CFA 4.0 specification that is backward compatible with CFA 2.0 (i.e. PCIe Gen3) cameras and readers of today, and forward compatible with CFA 4.0 (i.e. PCIe Gen4) cameras and readers of the future delivering the highest performance that you deserve.

Over 3700MB/s and 3000MB/s sequential read and write and 3300MB/s and 800MB/s sustained read and write performance from a 256GB Atlas Pro CFexpress 4.0 card measured on a Windows 11 computer with AMD Ryzen 9 processor mounted on a Gigabyte Technology x570 Aorus Master motherboard with 32GB of RAM.

 

Innergize Your Workflow with Highest Performance and Reliability

OWC Innergize™ is the first stage of the Capture to Completion™ ecosystem of OWC products designed to seamlessly propel professional photographers, videographers, and content creators to the highest level of workflow performance and reliability. This OWC custom-designed app is a complete health, performance, and field upgrade management tool when using OWC Atlas memory cards with OWC Atlas readers and reader equipped products.

                             Work with Maximum Confidence and Reliability

Health

Over time and use cycles, flash memory does wear out. Innergize verifies and reports the percentage of use life remaining. Now you can work with full confidence your OWC flash memory product will deliver the reliability you can trust.

Sanitize

Writes, deletes, and formatting all take their toll on memory cards. Innergize cleans and restores the flash memory performance of OWC memory cards so you can get the best results on every use.

Field Upgrade

When new cameras or firmware updates to existing cameras are introduced, they may not work properly with flash memory cards and drives. Innergize gives OWC memory card users the ability to quickly upgrade their firmware in the field for full compatibility, additional performance enhancements, and bug fixes for optimal reliability.