One Touch Looper Threading

Jet Air Technology

The AIR1800 has an easy one-touch looper threading that uses a blast of air for threading. With threading ports that are connected to the end of each looper by tubes, at the press of a button, the air sends the thread through the looper, so it’s a breeze to change threads.

4-Thread Overlock

The 4-thread overlock is one of the most commonly used stitches on a serger; it is the strongest of the construction stitches. Both loopers and two needles are used to complete the stitch, making it wider and sturdy because of the two needle stitches

Rolled Hems

The AIR1800 has pair of quick-change levers for the rolled hem feature, and a switch that will activate and deactivate the cutting knife before the edge is wrapped with thread (serged).

Knife Lock Lever

The Knife Lock Lever is located on the front of the machine, on the lower left side under the door. By moving the lever, you can cut, or trim fabric using the knife or disengage it for decorative stitch purposes

Safety Sensor and LED Error Indicator

The AIR1800 serger may display an error LED light and stop functioning due to one of the following: an open fabric cover; an open front cover; or the presser foot is raised

Quick Change Levers

The AIR1800 has pair of quick-change levers for the rolled hemstitch feature, and a switch that will activate and deactivate the cutting knife before the edge is wrapped with thread (serged)

Included Accessories:

  1. standard foot (on machine)
  2. 2-pcs needle set
  3. 4-pcs spool cap
  4. 4-pcs thread net
  5. screwdriver
  6. tweezers
  7. cleaning brush
  8. accessories box
  9. dust cover (not shown)
  10. foot controller

Ready to upgrade your sewing game?

Optional Feet (Sold Separately)*:

Add a professional touch to your sewing projects with our range of specialized sewing feet