AirMagnet Wi-Fi Site Survey - Overview

Visualize Coverage and Performance Differences Over Time

Wi-Fi environments are very dynamic and it is important to be able to verify changes in coverage and performance in the network to guarantee the best performance for the user. AirMagnet Survey’s Diff View feature allows side-by-side visualizing of differences between two separate surveys. This helps show how a site’s wireless environment has changed over time. This view is also a great option for our System Integrator customers to drive repeat business of validating the coverage and performance of the network on an on-going basis. Likewise, users can use this feature to quickly compare AirMagnet Planner results with actual site survey results. This information then can be used to fine tune the db losses for the building and environmental conditions within AirMagnet Planner for more accurate planning.

Integration with AirMagnet Planner

AirMagnet Planner is built into AirMagnet Survey PRO, providing a single, seamless application with the industry’s most complete approach to wireless LAN design, deployment and ongoing optimization for 802.11a/b/g/n/ac networks. With this integrated solution, AirMagnet Planner can be used to accurately design WLANs by modeling building construction materials/obstructions and 802.11 APs plus visualizing coverage across multiple floors, then validating the results with real-world data in AirMagnet Survey PRO. Using active end-user performance metrics, users can further perfect their planning models over time. With the new 802.11ac support, users are armed with the best migration guidance on how to phase in the new technology into the existing environment.

No other solution combines state-of-the-art predictive modeling with real-world performance data. Users also gain additional planning capabilities with the ability to test network plans against the AirWISE® engine for design requirements. AirMagnet Planner also integrates with AirMagnet Survey Express.