MSI G27C4X 27" Full HD Curved Screen Gaming LCD Monitor

Visualize your victory with MSI G27C4X Curved Gaming™ monitor. Equipped

with a 1920x1080, 250hz Refresh rate, 1ms response time panel, G27C4X will give you the competitive edge you need to take down your opponents. Built with AMD FreeSync™ Premium Technology, G27C4X can match the display's refresh rate with your GPU for ultra-smooth gameplay. Make sure you can hit your mark with all the latest technologies built-in the MSI Curved Gaming™ monitor for competitive play.

MSI Gaming monitors use a curved display panel that has a curvature rate of 1500R, which is the most comfortable and suitable for a wide range of applications from general computing to gaming. Curved panels also help with gameplay immersion, making you feel more connected to the entire experience.





250HZ REFRESH RATE + 1MS RESPONSE TIME

MSI monitors are equipped with a 250hz refresh rate + 1ms response time VA LED panel which has the most benefit in fast moving game genres such as first person shooters, fighters, racing sims, real-time strategy, and sports. These type of games require very fast and precise movements, which an ultra-high refresh rate and fast response time monitor will put you ahead of your competition.




Anti-Flicker Technology

Generic monitor displays normally have a flicker-rate of about 200-times per second, which is unnoticeable to the naked eye, but can cause fatigue over time. MSI Anti-Flicker technology provides a very comfortable viewing experience by reducing the amount of flicker.

From Edge to Edge

With a super narrow bezel, enjoy the best immersion possible in the latest games with a multi-monitor 180 degree setup. Enjoy better continuity between screens while playing games, working, or general computing.

Tear free, stutter free, fluid gaming

Gaming shouldn't be a choice between choppy gameplay or broken frames. With MSI gaming monitors, it doesn't have to be. Get fluid, artifact-free performance at virtually any framerate with AMD FreeSync™ technology.

SMART CROSS HAIR

The aim dot automatically changes color, making it visible at any time. If the color of the aim dot overlaps with the background color, it will be problematic for aiming.

The mostVivid Display

MSI gaming monitor is equipped with HDR technology that can produce images with more details, wider range of colors, and look more similar to what is seen by the human eye when compared to traditional monitor. Windows 11 Auto HDR supported, please check below link to learn more about Auto HDR and how to enable.

TRUE COLOR

The MSI Curved Gaming Monitor has more gamut coverage compared to general monitors. Gameplay colors and details will look more realistic and refined, to push immersion to its limits.

NIGHT VISION

Whether your entire screen is dark, or just a few portions have heavy shadows. Let the world's first smart black tuner brighten your day by bringing out the fine details in dark areas.