Royal Sovereign's Protection against Counterfeit Money

Maximum Security

This year, the Department of Treasury estimates there are over 70 million worth of fake bills in circulation! The RCD-BG1 ensures that every note you accept and put through the machine is being verified by the highest levels of protection. This machine is equipped with 5 levels of protection: MG, IR, Size Verification, Paper Quality, and Density & Thickness. This high security machine ensures that every bill is verified efficiently and accurately. Reject suspicious bills and reduce financial losses immediately!

Instant Results

Counterfeit detectors need to be quick and easy for the user to keep the line moving at the cash register. This model provides the user with immediate results. All the consumer needs to do is insert the bill into the currency feed and instantly see the results! This easy-to-use solution is a must-have for any business looking to protect themselves from financial loss.

Conclusive and Simple Results

Looking for a solution to keep the guessing out of the cashier’s hand? The RCD-BG1 does all the verifying for you with instant results that are easy for any user to comprehend. A ½ second scan time verifies the currency and takes the decision-making process of the user’s hands. Suspect bills are instantly rejected, and the user is provided with "FAIL". No need to spend time training and retraining employees on how to spot a counterfeit note!

RCD-BG1

User-Friendly

Businesses want the most user-friendly machine to deliver fast results. The RCD-BG1 is one of the most convenient detectors on the market. The RCD-BG1 accepts US currency in any direction. No need to train employees on how to insert the bill as the machine accepts any orientation. Most machines only accept bills one-way, however, the RCD-BG1 offers complete user convenience.

Dual Purpose Solution

The RCD-BG1 serves as a bill counter as well as a counterfeit detector. This machine can keep a running record of the total count and value of bills. A 2-in-1 solution that provides a detailed count report for record keeping and verifies the currency at the same time.

Compact Design

Tired of large bulky counterfeit detectors taking up space near the register? With its compact and portable design, the RCD-BG1 can fit perfectly next to a register or cash handling machine. No more bulky products that take up a lot of space. Optimize space next to a register with this high-quality solution.