![](https://content.etilize.com/rich-marketing/en_us/1031512862/Q0lWELMSTmJ8sBEjs0iv_cZ9RKVF.jpg)
Turn Coaxial Wiring into a High Speed Network
The Bonded MoCA 2.0 Network Adapter is a high-speed bridge that in conjunction with a router, delivers gigabit Ethernet networking access anywhere you have a coaxial port. It works right over the home’s existing coaxial wires, and installs in minutes.
![](https://content.etilize.com/rich-marketing/en_us/1031512862/kj2FSOeXTby3NThDXLrM_4MMauGy.jpg)
![Instant Performance Boost for your Home Network with Gigabit Speeds<br></br>When your home is faced with Wi-Fi challenges, like deadspots or interference, Actiontec’s ECB6200 Bonded MoCA 2.0 Network Adapter brings an instant performance boost to the home network, ensuring uninterrupted and pristine HD video, online gaming, and high speed networking.](https://content.etilize.com/rich-marketing/en_us/1031512862/K1l3YCjPTeeECJb3dLha_XdgWJlw.jpg)
Instant Performance Boost for your Home Network with Gigabit Speeds
When your home is faced with Wi-Fi challenges, like deadspots or interference, Actiontec’s ECB6200 Bonded MoCA 2.0 Network Adapter brings an instant performance boost to the home network, ensuring uninterrupted and pristine HD video, online gaming, and high speed networking.
When your home is faced with Wi-Fi challenges, like deadspots or interference, Actiontec’s ECB6200 Bonded MoCA 2.0 Network Adapter brings an instant performance boost to the home network, ensuring uninterrupted and pristine HD video, online gaming, and high speed networking.
![The Latest Bonded MoCA Technology for Gigabit Speeds<br></br>With support for the latest bonded MoCA 2.0 standard, the ECB6200 bonds MoCA channels to support speeds up to 1 Gbps**, more than enough bandwidth for HD video, online gaming, and other demanding applications. You get the reliability and performance of a wired connection without the expense of wiring the home for Gigabit Ethernet.](https://content.etilize.com/rich-marketing/en_us/1031512862/qHZHwF9bS42ICGqf0obL_DWzfgK4.jpg)
The Latest Bonded MoCA Technology for Gigabit Speeds
With support for the latest bonded MoCA 2.0 standard, the ECB6200 bonds MoCA channels to support speeds up to 1 Gbps**, more than enough bandwidth for HD video, online gaming, and other demanding applications. You get the reliability and performance of a wired connection without the expense of wiring the home for Gigabit Ethernet.
With support for the latest bonded MoCA 2.0 standard, the ECB6200 bonds MoCA channels to support speeds up to 1 Gbps**, more than enough bandwidth for HD video, online gaming, and other demanding applications. You get the reliability and performance of a wired connection without the expense of wiring the home for Gigabit Ethernet.
![Trusted by Millions Most of the leading broadband <br></br>companies rely on coaxial networks in the home because it is very fast and extremely reliable. Join the millions of homes in North America that are taking their HD video streaming and online gaming to the next level with an Actiontec MoCA solution.](https://content.etilize.com/rich-marketing/en_us/1031512862/96sZ4MKPRDinB9QVD8hn_khnYGB1.jpg)
Trusted by Millions Most of the leading broadband
companies rely on coaxial networks in the home because it is very fast and extremely reliable. Join the millions of homes in North America that are taking their HD video streaming and online gaming to the next level with an Actiontec MoCA solution.
companies rely on coaxial networks in the home because it is very fast and extremely reliable. Join the millions of homes in North America that are taking their HD video streaming and online gaming to the next level with an Actiontec MoCA solution.
* Actual speeds will vary depending on the condition and noise found on the coaxial wiring. 1.06 Gbps is the maximum throughput.
**Requires that your router support bonded MoCA 2.0.
**Requires that your router support bonded MoCA 2.0.
Easy to Install
![<center>Step 1 </br>
Simply connect a coaxial cable from your Router to a nearby Coax outlet.</center>](https://content.etilize.com/enhanced-overview/en_us/148825/nYVS4cxQfOg8XZvcF81i_waqas.jpg)
![<center>Step 2 </br>
Add another MoCA adapter to the HDTV, set top box or other device.</center>](https://content.etilize.com/rich-marketing/en_us/1031512862/BJs23qsmQEagfCwsdIyi_nQgfj0QeSCKlOA28NRDQ_Dvc2ECB6200.jpg)
![<center>Step 3 </br>
Make sure the Power and Coax LEDs (or lights) are solid green.</center>](https://content.etilize.com/rich-marketing/en_us/1031512862/CmbRuFwAR5mmNMouyVBu_VUDUOzUQUObpkX4k7dOX_newECB6200_beauty_LEDcircle.jpg)
Product Family
Good | Better | Best | |
---|---|---|---|
MoCA Physical Network Speeds | Up to 275 Mbps PHY Rate or 175 Mbps Throughput | Up to 700 Mbps PHY Rate or 500 Mbps Throughput | Up to 1.4 Gbps PHY Rate or 1 Gbps Throughput |
MoCA Version | MoCA 1.1 | MoCA 2.0 | Bonded MoCA 2.0** |
Model # | ECB2500C | ECB6000 | ECB6200 |
* Actual speeds will vary depending on the condition and noise found on the coaxial wiring. 1.06 Gbps is the maximum physical data rate.
**Requires that your router support bonded MoCA 2.0
**Requires that your router support bonded MoCA 2.0