Swingline Portable Electric Stapler, 20 Sheets, Black
A speedy, space-saving electric model Speed, convenience and flexibility are the key features of the Portable Electric Stapler. This compact model can easily be taken on the road. It has the ability to staple up to 20 sheets at a time and you don't even need an outlet. An AC adapter is included, but the Portable Electric Stapler delivers the same great performance when run on 6 AA batteries. (Batteries not included) This electric stapler has a quiet motor so that it can be used in any space without interruption. A low staple indicator helps ensure that you can work uninterrupted as well by anticipating when you will need to refill. A precision alignment guide, up to 1-1/2", is also included to ensure consistency of staple placement. The space-saving electric stapler is ideal for last minute, unexpected stapling needs and is especially handy when you need to finish up your work while traveling. It is highly efficient and will provide reliable stapling for the long term. For best performance, use the Portable Electric Stapler with S.F. 4 Premium Staples.