Acer Chromebook Plus Enterprise 515

An Acer Chromebook Designed for Your Dynamic Lifestyle

Acer Chromebook Plus Enterprise 515 (CBE595-2/CBE595-2T)
Acer Chromebook Plus Enterprise 515 (CBE595-2/CBE595-2T)
Equipped with Intel ® Core™ Processor 1 and a 15.6” full HD display 1 the Acer Chromebook Plus Enterprise 515 powers your workforce, unleashes your organization’s creativity, and enables offline work from anywhere.
300x150-1-34
300x150-2-35
300x150-3-35
300x150-4-35
300x150-5-28

Do more than you thought you could

Powered with Intel® Core™ processor1 this Acer Chromebook Plus offers more than just a performance score, advancing real-world computing and delivering efficient multi-tasking.

Chromebook_plus_Enterprise_515_KSP01
Chromebook_plus_Enterprise_515_KSP01-1_1440x800
Secure by design

ChromeOS devices and Chrome browser deter end users from falling hostage to harmful attacks and mitigate impact if one prevails.

Chromebook_plus_Enterprise_515_KSP01-2_1440x800
Biometric Security

Say goodbye to passwords and embrace the power of biometric authentication secure employee access to device.

Chromebook_plus_Enterprise_515_KSP01-3_1440x800
Stay Productive Offline

File Sync, available with Acer Chromebook Plus, automatically syncs files to File Manager, so Google Docs, Sheets, and Slides are always accessible — even when offline2.

More Power, So You Can Do More

With 2X the power, speed, memory, and storage of other devices, and a high-definition camera and display, your people are empowered to do their best work3.

Chromebook_plus_Enterprise_515_KSP02
Chromebook_plus_Enterprise_515_KSP02-1_1440x800
Everything you need to get anything done

ChromeOS gives employees access to the productivity and video conferencing apps they prefer, like Zoom, Slack, Meet Google Workspace, Microsoft 365®5, and Teams. Managed Google Pay allows IT to curate and deploy top enterprise apps and private apps.

Chromebook_plus_Enterprise_515_KSP02-2_1440x800
Software and hardware features to activate worker productivity

Our modern, cloud-first OS coupled with 2X the power, speed, memory, and storage3 of our devices, empowers your people to do their best work, whether they’re in-office, remote – or anywhere in between.

Chromebook_plus_Enterprise_515_KSP02-3_1440x800
Get more done at a lower cost

Reduce your cost of ownership with devices that have a 245% ROI over three years2.

Full HD. Fully Immersive

A 15.6” FHD 1080p narrow bezel display with anti-glare and optional touch captures vibrant details, whether you’re editing photos, or streaming your favorite shows.

 

84.1%

Screen-to-body ratio1

 

300 nits

Brightness1

 

16:9

Aspect ratio

Chromebook_plus_Enterprise_515_KSP03

Crystal Clear Calls

Acer Chromebook Plus has a 1080p FHD webcam and built-in AI-powered video call tools that enhance clarity and lighting, to look your best on any video call app.

Chromebook_plus_Enterprise_515_KSP04
Chromebook_plus_Enterprise_515_KSP04-1_1440x800
Privacy Camera Shutter

Confidently navigate the digital landscape, knowing your privacy is safeguarded.

Chromebook_plus_Enterprise_515_KSP04-2_1440x800
Acer TNR

Capture better images by detecting, diagnosing, and blending, producing improved quality images in low-light conditions.

Chromebook_plus_Enterprise_515_KSP04-3_1440x800
Auto Facial Exposure Camera

Automatically adjusts the exposure settings based on the lighting conditions of the subject’s face.

Connect with Ease

With fast WiFi 6E1 and Bluetooth 5.21 connectivity, connect to all your favorite accessories and devices.

 

Thunderbolt 4

Type C

 

USB 3.2 Gen 1

Type A

 

2.0

HDMI

Chromebook_plus_Enterprise_515_KSP05

ChromeOS

Deploy, manage, and secure your devices with Chrome Enterprise Upgrade. Chrome Enterprise Upgrade unlocks the built-in business capabilities of ChromeOS. Drop ship devices directly to employees ready to be signed in with zero-touch enrollment.

Chromebook_plus_Enterprise_515_KSP06
Chromebook_plus_Enterprise_515_KSP06-1_1440x800
Chrome Enterprise Upgrade

Chrome Enterprise Upgrade simplifies the way you run your business. Cut costs, simplify operations, reduce security risks, and greatly lower required IT resources by being able to deploy, update and manage all your devices at any scale.

Chromebook_plus_Enterprise_515_KSP06-2_1440x800
Zero-Touch Enrollment

Featuring zero-touch enrollment, IT departments will be able to drop ship ChromeOS devices that will be automatically enrolled into enterprise administration as soon as the user connects to the internet.

Sustainability

Featuring recycled materials, sustainable packaging, an energy-efficient design, and EPEAT registration6 this Acer Chromebook Plus embodies the spirit of our Earthion initiative to reduce waste across the lifetime of the device.

Chromebook_plus_Enterprise_515_KSP07
Chromebook_plus_Enterprise_515_KSP07-1_720x400​
Less Plastic Waste in the Ocean

We use recycled ocean-bound plastic in the OceanGlassTM touchpad of this Acer Chromebook Plus. The touchpad gives you a sleek, glass-like tactile feel as your fingers scroll across its surface

Chromebook_plus_Enterprise_515_KSP07-2_720x400
Conserve Natural Resources

Our molded pulp packaging uses recycled paper, cardboard, and other natural fibers, offering greater sustainability benefits than traditional plastic and Styrofoam packaging.

1 Specifications of this device may vary depending on model and/or region.
2 IDC Business Value Snapshot, sponsored by Google ChromeOS, The Business Value of ChromeOS, doc #US50055223, January 2023
3 When compared to top selling Chromebooks from July 2022 to Dec 2022.
4 You must be connected to the internet to set up this feature. Download required. Must have available storage space in Drive.
5 Additional functionality available with Microsoft 365 ® subscription. Microsoft, Excel and PowerPoint are registered trademarks of Microsoft Corporation.
6 EPEAT ® registration varies by country. See http://www.epeat.net/ for registration status for each country.
Battery life may vary depending on model and configuration. Based on Google power_LoadTest. Actual battery life varies by model/configuration.
MIL-STD 810G/H is a testing protocol conducted in controlled settings and does not guarantee future performance in all situations. Do not attempt to simulate these tests, as damage resulting from this will not be covered by Acer's standard warranty